Frick_Logo_Full_Color
Johnson Controls  |  Frick


Our redesigned FPHE

The latest in insulated penthouse evaporator technology 

 

1. Improved accessibility and reliability

We’ve added larger access doors and moved it closer to ground level. Now, a technician can walk directly into the unit. Servicing your evaporator will be easier than ever.

2. Improved Serviceability

Our new junction box is now on the outside. It contains the unit’s 120 V circuitry, so there’s no longer a need to run low voltage wires through the walls of your evaporator. Not only does this improve serviceability but also the performance of the unit, as moisture and air will have nowhere to escape or infiltrate.

3. Safety is paramount

The FPHE-R design includes a weatherproof membrane over the entire rooftop. Your unit is protected from the elements, thus eliminating risk of ice formation inside the unit, which could be a safety hazard inside your facility.

4. Smart new look

We’ve retired the white box. Our new insulated penthouse evaporator has a textured metal casing that is darker in color, maintains its appearance better and isn’t prone to scratches. It will be the pride and joy of any rooftop.


To learn more, please contact us by filling out the form on the right.
 

Get in Touch to learn more about our new FPHE

 

https://www.johnsoncontrols.com/legal/terms

 
jci footer NEW
jci tagline best clear no padding (NO JCI)
johnson-controls_165px
© 2022 Johnson Controls. All Rights Reserved.Legal  |  Privacy
Legal  |  Privacy